990-1000015-001

Prepare Internal Signal Cables Between MBC and UPS

  1. Remove the signal cable cover from the UPS. Open the front door of the maintenance bypass cabinet and remove the three front panels from the maintenance bypass cabinet.

    Front View of the UPS and Maintenance Bypass Cabinet

  2. Remove the protection cover over the non-Class 2/non-SELV terminals.

    Front View of the UPS

  3. Only for top cable entry: Route the non-Class 2/non-SELV signal cables through the top opening and down to the non-Class 2/non-SELV terminals as shown.

    Front View of the UPS and Maintenance Bypass Cabinet

  4. Only for bottom cable entry: Route the non-Class 2/non-SELV signal cables through the bottom opening and up to the non-Class 2/non-SELV terminals as shown.

    Front View of the UPS and Maintenance Bypass Cabinet

  5. Fasten the signal cables with cable ties as shown.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?