990-5912E-001

Connect the Power Cables for a 3:3 UPS System

NOTE: For a simplified 1+1 parallel system, install the power cables from the two UPSs on the front and rear side of the busbar using the same bolt.
  1. Connect the PE cables to the PE busbar.

    GVSBPSU10K20H

    GVSBPSU20K60H and GVSBPSU80K120H

  2. Do one of the following:
    • For single mains: Connect the input cables from utility/mains.
    • For dual mains: Connect the bypass cables from utility/mains.
  3. Do one of the following:
    • For single mains: Connect the UPS input cables.
    • For dual mains: Connect the UPS bypass cables.
  4. Connect the UPS output cables.
  5. Connect the load cables.

    GVSBPSU10K20H

    GVSBPSU20K60H and GVSBPSU80K120H (for Galaxy VS)

    GVSBPSU20K60H and GVSBPSU80K120H (for Easy UPS 3S, Easy UPS 3S Pro, Easy UPS 3M)

    NOTE: For Easy UPS 3S, Easy UPS 3S Pro, and Easy UPS 3M, when the neutral jumpers are removed, it is mandatory to connect the neutral (N) cables from the UPS output.
  6. Fasten the cables with cable ties (provided) to the cable reliefs in the left side, top, and bottom of the maintenance bypass panel.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?