990-5912E-001

Final Installation

  1. Close the inner door and fasten it with the screws.
  2. Add labels to the disconnect device indicator lamps, the disconnect devices, and the diagram label according to your system. The labels are provided with this manual.

    Labels in Single System – Single Mains

    Labels in Single System – Dual Mains

    Labels in Simplified 1+1 Parallel System – Single Mains

    Labels in Simplified 1+1 Parallel System – Dual Mains

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?