990-5912E-001

Remove the Neutral Jumpers

NOTE: The neutral jumper makes a bolted connection of the neutral so that the neutral is not disconnected when the 4-pole disconnect devices are opened.
NOTE: Only remove the neutral jumpers in a Galaxy VS installation, if this is a local requirement. Removal of the neutral jumpers is an option for a Galaxy VS installation.
NOTE: Always remove the neutral jumpers in an Easy UPS 3S/3S Pro installation or in an Easy UPS 3M installation. Removal of the neutral jumpers is mandatory for an Easy UPS 3S/3S Pro or an Easy UPS 3M installation.
  1. Remove the neutral jumpers from the disconnect devices.

    GVSBPSU10K20H

    GVSBPSU20K60H

    GVSBPSU80K120H

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?