990-5993C-001

Install Batteries in the Modular Battery Cabinet in 400 V Systems

  1. Remove the plate in front of the battery shelves.
  2. Holding the handle, install the battery modules one string at a time from the bottom and up.
  3. Push down the handle of each battery module and fasten with the provided screw in front of the battery module.

    Front View of Battery Module

  4. Remove the shrink tubes from the power terminals and connect the power terminals to the batteries.
  5. Reinstall the plate in front of the battery shelves.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?