990-5993C-001

Connect Cables between the Easy UPS 3S and the Modular Battery Cabinet

NOTE: Route the signal cables separately from the power cables.
  1. Remove the conduit box from the rear side of the modular battery cabinet.

    Rear View of the Modular Battery Cabinet

  2. Rotate the conduit box and install.
  3. Remove the right or left side panel.

    Front View of the Modular Battery Cabinet

  4. Connect the supplied battery cables to the busbars:
    • 10–20 kVA UPS: WH100138 (Bat+), WH100139 (N), WH100140 (Bat-), WH100145 (PE)
    • 30–40 kVA UPS: WH100141 (Bat+), WH100142 (N), WH100143 (Bat-), WH100146 (PE)

    Right Side View of the Modular Battery Cabinet

  5. If more than one modular battery cabinet is part of the installation, connect the battery cables between the modular battery cabinets.
  6. Install the temperature sensor E3SOPT003 (if available).

    Right Side View of the Modular Battery Cabinet

  7. Route the battery temperature sensor cables through the conduit box to the UPS. Disconnect the cables from J2–1 and J2–2 and connect the battery temperature sensor.
  8. Reinstall the side panel.
  9. Fasten the cables to the cable reliefs.

    Rear View of the Modular Battery Cabinet

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?