990-5940H-001

Connect the Power Cables in the 20 kVA 400 V / 10 kVA 208 V UPS

  1. Ensure that all breakers are in the OFF (open) position.
  2. Remove the conduit box cover.

    Rear View

  3. In dual mains systems, remove the three single mains brackets.
  4. Route the power cables through the bottom of the conduit box.
  5. Connect the PE cable to the PE terminal.
  6. Connect the input cables, output cables, and bypass cables (if applicable).
  7. Connect the battery cables if the UPS should have external batteries for extended runtime.
    NOTE: Ensure that the type and number of blocks are the same as the internal batteries.
  8. Reinstall the conduit box cover.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?