990-5940H-001

Recommended Bolts and Cable Lugs

Cable Size (mm²)

Bolt Size

Cable Lug Type

Note

6

M5

KST TLK6-5

If the recommended lug type is not available, use a local M5 lug type as a substitute.

8

M5

KST RNBS8-5

10

M6

KST TLK10-6

If the recommended lug type is not available, use a local M6 lug type as a substitute.

16

M6

KST TLK16-6

25

M6

KST DRNB6-25

35

M6

KST TLK35-6

50

M8

KST TLK50-8

If the recommended lug type is not available, use a local M8 lug type as a substitute.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?