990-66302-001

Installation Procedure

NOTE: This procedure describes installing the IP40 kit after power cabling and signal cabling is completed. Rear access is required to install the IP40 kit on the UPS.
DANGER
The UPS must be completely turned off while the kit is being installed.
Failure to follow these instructions will result in death or serious injury.
  1. Follow the UPS installation manual to install the UPS.
  2. Install the IP40 Front Protection on the UPS.
  3. Install the IP40 Rear Protection on the UPS.
  4. Install the IP40 Side Protection on the UPS.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.