990-66302-001

Install the IP40 Rear Protection on the UPS

DANGER
The UPS must be turned completely OFF before performing this procedure.
Failure to follow these instructions will result in death or serious injury.
  1. Remove the M4 screws from the rear panels. Save the screws for reuse.
    NOTE: Do not remove the rear panels from the UPS.

    Rear View

  2. Install the new IP40 protection over the existing rear panels with the reused M4 screws.

    Rear View

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.