990-66302-001

Install the IP40 Side Protection on the UPS

DANGER
The UPS must be turned completely OFF before performing this procedure.
Failure to follow these instructions will result in death or serious injury.
  1. Remove the left and right side panels from the UPS. Save the M4 screws for reuse.
  2. Attach the protective sponge strips on both the left and right sides of the UPS.

    Side View

  3. Reinstall the left and right side panels on the UPS with the reused M4 screws.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.