990-92223B-001

Backfeed Box One Line Drawing

Instruction to end user as follows:
a) Easy UPS backfeed box having a rated conditional short-circuit current and not exceeding 10 kA r.m.s.
b) Easy UPS backfeed box shall be protected by current-limiting devices having a cut-off current not exceeding 17 kA with the maximum allowable prospective short-circuit current at the terminals of the incoming circuit of the ASSEMBLY.
Instruction to end user as follows:
a) Easy UPS backfeed box having a rated conditional short-circuit current and not exceeding 10 kA r.m.s.
b) Easy UPS backfeed box shall be protected by current-limiting devices having a cut-off current not exceeding 17 kA with the maximum allowable prospective short-circuit current at the terminals of the incoming circuit of the ASSEMBLY.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?