990-92223B-001

Mount the Backfeed Box to the Wall

CAUTION
Risk of injury or equipment damage
  • Mount the backfeed box to a wall or a rack that is structurally sound and able to support the weight of the unit.
  • Use appropriate M10 hardware (not supplied) to mount the backfeed box to the wall.
Failure to follow these instructions can result in injury or equipment damage.
  1. Measure and mark the four mounting hole locations on the wall.

    SP3OPT008

    SP3OPT009

    SP3OPT010

  2. Drill holes in each of the four marked locations.
  3. Mount the backfeed box to the wall.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?