990-92223B-001

Connect the Input Power Cables to the Input Backfeed Box

  1. Connect the PE cables.
  2. Connect the UPS input cables (L1, L2, L3, N).
  3. Connect the input cables (L1, L2, L3, N).
  4. Reinstall the front plate with the screws.
  5. Close and lock the front door.

    SP3OPT008 (Input Only)

    SP3OPT009 (Input Only)

    SP3OPT010 (Input Only)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?