990-66229A-001

Connect the Power Cables in the 30-40 kVA UPS

  1. Ensure that all disconnect devices are in the OFF (open) position.
  2. Remove the conduit box cover.

    Rear View

  3. Remove the transparent protective cover from the terminal blocks.

    Rear View

  4. In single mains systems: Perform one of the following to prepare for the earthing system:
    • For TN-C earthing system: The L-shaped jumper is provided in the paper bag attached to the installation manual. Remove the fourth V-shaped jumper from the terminal blocks and replace it with the provided L-shaped jumper in the same position.

      Rear View – TN-C Earthing System (Single Mains)

    • For non TN-C earthing system: No action is needed to prepare for the earthing system.

  5. In dual mains systems: Perform one of the following to prepare for the earthing system:
    • For TN-C earthing system: The L-shaped jumper is provided in the paper bag attached to the installation manual. Remove the four V-shaped jumpers from the terminal blocks and install the provided L-shaped jumper in the fourth position in the terminal blocks.

      Rear View – TN-C Earthing System (Dual Mains)

    • For non TN-C earthing system: Remove the four V-shaped jumpers from the terminal blocks.

      Rear View – TN-C Earthing System (Dual Mains)

  6. Cut holes on the cable brush plate. 

    Rear View for 30 kVA UPS

    Rear View for 40 kVA UPS

  7. Route the power cables through the conduit box.
  8. Connect the PE cable to the PE terminals.

    Rear View

  9. Connect the battery cables and the output cables.
  10. Connect the input cables and the bypass cables (in dual mains systems).
  11. Reinstall the transparent protective cover over the terminal blocks.

    Rear View

  12. Reinstall the conduit box cover.

    Rear View

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?