990-66229A-001

Connect the Signal Cables

Overview of Signal Connection Terminals in the 10-20 kVA UPS

Overview of Signal Connection Terminals in the 30-40 kVA UPS

  1. Slot for network management card (NMC)

  2. Slot for optional dry contacts board

  3. Cold start button (optional)

  4. Parallel connection ports

  5. USB port (for service)

  6. RS485 port

  7. CAN

  8. Input contacts and output relays (dry contacts)

NOTE: Route the signal cables separately from the power cables and route the Class 2/SELV cables (A to C, E to H) separately from the non-Class 2/non-SELV cables. Non-Class 2/non-SELV cables (D) should be rated for 300 V.
NOTE: The recommended cable size for the signal cables is 0.5 mm2.

NOTE: The maximum length for Modbus cables is 80 m.

NOTE: Please refer to the following illustrations for the SELV and non-SELV cable routing.

SELV and Non-SELV Cable Routing for 10 - 20 kVA UPS



SELV and Non-SELV Cable Routing for 30 - 40 kVA UPS

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?