990-6427-001

Connect the Power Cables

  1. Route the ground cables through the top or bottom and connect.
  2. Route the input cables through the bottom and connect to the terminals of the MBB breaker.
  3. Route the output cables from the three UPSs through the bottom and connect to the terminals of the SIB.
  4. Route the system output cables through the top and connect the system output cable landings.
  5. Fasten the cables with the cable ties (provided) to the cable reliefs.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?