990-6427-001

Connect the Signal Cables

NOTE: Route the signal cables separately from the power cables.
  1. Remove the plastic cover of the maintenance bypass breaker MBB to get access to the auxiliary switches.
  2. Connect signal cables 22 AWG (not supplied) between the maintenance bypass breaker MBB and the UPSs.
  3. Route the signal cables through the top or bottom of the parallel maintenance bypass panel and fasten the signal cables to the cables reliefs.

    Top Cable Entry System

    Bottom Cable Entry System

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?