Discovery of Wireless Devices Through Webpages
Presentation
Wireless devices installed in the Panel Server system can be discovered through the EcoStruxure Panel Server webpages by using one of the methods described: Automatic or Selective.
-
Automatic (default): discovers wireless devices in the Panel Server system
-
Selective: discovers only the wireless devices belonging to a selective list. You can enter the list manually in the webpages or you can upload a prepared file containing the list.
The Protect Plus function allows you to launch a discovery with heightened security by using the 36-character install code of 16-character RF-ID devices. The following device families have a 16-character RF-ID:
-
PowerTag Control
-
PowerLogic HeatTag
-
PowerLogic PD100
-
MasterPacT MTZ with MicroLogic Active AP or EP control unit
-
Exiway Link
With Protect Plus selected (selected by default), automatic discovery is available for 8-character RF-ID devices, for example, PowerTag Energy. To discover 16-character RF-ID devices, use a selective list which includes the 36-character install code of the devices.
With Protect Plus deselected, all devices can be discovered without benefiting from the heightened security level.
Automatic Discovery of Wireless Devices Through Webpages
The following table indicates automatic discovery availability depending on Protect Plus setting:
| Device type | Example | Discovery available | |
|---|---|---|---|
| Protect Plus selected | Protect Plus deselected | ||
|
8-character RF-ID |
PowerTag Energy |
Yes |
Yes |
|
16-character RF-ID |
PowerLogic HeatTag |
No |
Yes |
To perform an automatic discovery of wireless devices through webpages, proceed as follows:
-
Log in to the Panel Server webpages (see how to access the webpages).
-
Navigate to and click Automatic.
-
Click Start to scan the environment and discover available wireless devices.
Result: Devices appear in the list of discovered wireless devices and in the device tree view as they are discovered.
In certain cases, devices may not be fully discovered by the Panel Server. In the Rejected Discovery table, a column labelled Status gives the cause of the rejected discovery.
For devices indicating Install code not provided, use a selective list to enter the missing information and launch a selective discovery.
NOTE: A popup message indicates if the network occupancy is high or saturated and suggests solutions. If action is required, navigate to . -
If required, you can select the wireless device in the device tree view and click Locate to find the device in the panel.
Result: The status LED of the selected device blinks fast green in the panel.
-
If one of the located wireless devices is not part of your system, click Delete to reject the device.
-
Configure the wireless devices.
Selective Discovery of Wireless Devices Through Webpages
Selective discovery uses the RF-ID of a wireless device to perform a discovery.
The following table indicates selective discovery availability depending on Protect Plus setting:
| Device type | Example | Discovery available | |
|---|---|---|---|
| Protect Plus selected | Protect Plus deselected | ||
|
8-character RF-ID |
PowerTag Energy |
Yes |
Yes |
|
16-character RF-ID |
PowerLogic HeatTag |
With install code* |
Yes |
|
* Recommended to benefit from heightened security during installation |
|||
To perform selective discovery of wireless devices through webpages, proceed as follows:
-
Log in to the Panel Server webpages (see how to access the webpages).
-
Navigate to and click Selective.
All and only the wireless devices in the selective list can be discovered by the Panel Server. The Panel Server uses the RF-ID of each device to discover it.
-
Upload a prepared list file by clicking Upload file, or fill in the table that opens with the following information for each device in the selective list:
-
Virtual server ID in the range 1 to 254 (optional). If the ID is not specified, the Panel Server assigns the first available value.
-
Install code (with Protect Plus enabled) for applicable devices
IMPORTANT: Uploading a prepared selective list erases any data that has been added manually to the selective list in the webpages. -
Click Start to scan the environment and discover the wireless devices in the list.
Result: Devices appear in the list of discovered wireless devices and in the device tree view as they are discovered.
In certain cases, devices may not be fully discovered by the Panel Server. In the Rejected Discovery table, a column labelled Status gives the cause of the rejected discovery. Check the cause and correct the issue before relaunching the selective discovery.
If the device is not discovered and does not appear in the Rejected Discovery table, refer to Troubleshooting webpages.
NOTE: A popup message indicates if the network occupancy is high or saturated and suggests solutions. To check the network occupancy, navigate to .
Virtual Server ID
A virtual ID address is applied during the discovery process with the Panel Server. The first virtual server address ID is allocated to the first discovered device and incremented by one for each device discovered. By default, virtual server IDs allocated to wireless devices start from 100.
When using the selective discovery process, the virtual server IDs can be defined in the selective list. If they are not defined in the list, virtual server IDs are allocated in order of discovery, as above.
The virtual server ID assigned to the wireless devices can be changed after the discovery process is done.
Defining the List of Selected Devices
The selective list is a csv file that lists the selected wireless devices to be uploaded on the Panel Server webpages. Each row in the csv file contains the data for one device in the following format, separated by semi-colons:
-
RF-ID with 0x prefix (mandatory)
-
Virtual server ID (optional)
-
Install code with 0x prefix (for use with Protect Plus)
Example of csv file:

Finding the Device RF-ID and Install Code
To obtain the RF-ID and install code of a device, scan the QR code of the device. Follow the link to the Go2SE landing page of the device and click More details to find the relevant information:
- zb = RF-ID (8 or 16 characters)
- ic = install code made up of 36 characters (depending on the device)