DUG_PowerTag Control_ELKO_WH-00

Installing the device

Refer to the installation instruction supplied with this product.

It is recommended to install the PowerTag within 3 metres of the Wiser Hub for best results. Signal quality is best maintained when there are no big obstructions (thick walls, metal cabinets etc.) between the PowerTag & your Wiser Hub. This provides a good network strength and helps to prevent online/offline issues, which might result in corrupting data.

Refer installation video: How to Install PowerTag Control - IO Module
This video is applicable for installation of PowerTag driving an Impulse relay using “remote indication auxiliary and 2 feedback loop wires”. Wherein for the PowerTag driving a contactor does not “require remote indication auxiliary and 2 feedback loop wires”.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?