DUG_SmartBlinds Push_WH-00

Blind Control Switches

NOTE: To pair a Wireless switch with one blind control switch, follow the steps up to step 3. To continue with a second blind control switch, follow the next steps.
  1. Remove the rocker from the Wireless switch.
  2. Short press the top-right push button 5 times in quick succession on the Wireless switch.
    The status LED blinks green.
  3. Short press the first blind control switch 5 times in quick succession.
    The status LED blinks green.

    The shutter will move up and down a few times during the pairing process. The status LED stops blinking green on the Wireless switch, and the blind control switch indicates that the pairing is successful.
    IMPORTANT: Check if the pairing was successful before you continue with the left channel.
  4. Short press the top-left push button 5 times in quick succession on the Wireless switch.
    The status LED blinks green.
  5. Repeat step 3 on the second blind control switch.
    The shutter will move up and down a few times during the pairing process. The status LED stops blinking green on the Wireless switch, and the blind control switch indicates that the pairing is successful
  6. Set up the shutter calibration manually.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.