DUG_SmartBlinds Push_WH-00

Pairing the device with the Wiser Hub

Using the Wiser Home app, pair your blind control switch with the Wiser Hub to access and control the blind control switch.
  1. On the Home screen, tap .
  2. Tap Devices > > Shutters > 1-Gang Switch.
    TIP: You can also navigate by tapping Control > > Shutters > 1-Gang Switch.
  3. Tap Scan QR code and allow the Wiser Home app to access your camera. Then, scan the QR code located on the device.
    NOTE: If you are unable to find the correct QR code, tap I can't find the correct QR code to pair the device manually and proceed to step 4.

    If the QR code is incorrect, a message Incorrect QR code scanned will appear. Tap I can't scan the QR code and choose one of the following options:

    • (A): Enter the Mac Address/EUI-64 and Install Code, then tap Connect. The app will verify if the Mac Address/EUI-64 and Install code are valid.

    • (B): Tap this option if you are unable to find the Mac Address/EUI-64 and Install code.

  4. Once the device is validated, tap Next, short-press the push button on the blind control switch 3 times and make sure that the LED blinks amber.

    Wait for a few seconds until the LED turns green and the app confirms that the device is joined.
    NOTE: If the LED is blinking green and red, see the instructions by tapping LED blinking green and red?.
  5. Tap , enter a name of the device.
  6. Tap Next and assign the device to a new room or an existing room and tap Submit.
  7. Tap Next > and select a Device Type:
    • Shutter: Proceed to step 8.
    • Shutter with tilting slats: Proceed to step 9 to 11.
  8. Tap Shutter > Next and enter the open/close duration of shutter. Refer to Setting default run time.
  9. Tap Shutter with tilting slats > Slat Type , select a slat type and tap Set:
    • Horizontal
    • Tilted
    • Vertical
  10. Tap Next and enter the following durations:
    1. Open duration: Time taken to open the shutter.
    2. Close duration: Time taken to close the shutter.
    3. Tilt duration: Time taken to rotate the slats completely from closed to open position.
  11. Tap Submit.

    After you pair the device, a success screen appears with the following options:

    • + Add New Device: Tap to continue pairing more devices.

    • Start Using Your Device: Tap to start using the paired device.

    NOTE: The success screen appears only if you are logged in as a Home Owner.

    Once the pairing process is completed, the device name is listed on the Control tab under the All and Room tabs.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.