DUG_SmartBlinds Push_WH-00

Setting the seasonal comfort mode

Using the Wiser Home app, you can change the configuration of the seasonal comfort mode.
Pre-requisite:

On the Home screen, tap > Smart Modes > Seasonal Comfort Mode.


The Seasonal Comfort Mode set-up page is displayed, where you can update the following configurations:
To change the configuration of the seasonal comfort mode:

A

Seasonal Comfort Mode: Tap the toggle switch to turn the seasonal comfort mode ON/OFF.

B

Shutters: Tap to change the orientation and location of the shutters in the Wiser Home app. Refer to Changing the shutter orientation and location for more details.

C

Temperature: Tap to change the threshold inside and outside temperatures in the Wiser Home app. Refer to Setting the threshold temperature for more details.

D

Time: Tap to change the start and end time of the seasonal comfort mode in the Wiser Home app. Refer to Setting the start and end time for more details.

E

Light (LUX) sensors: Tap to change the orientation of the light sensors in the Wiser Home app. Refer to Changing the orientation of the light sensors for more details.

F

Outside temp sensors: Tap to change the orientation of the outside temperature sensors in the Wiser Home app. Refer to Changing the orientation of the outside temperature sensors for more details.

G

Other room sensors: Tap to manage the shutter operation without temperature sensors. Refer to Managing the shutter operation without temperature sensor for more details.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.