DUG_SmartBlinds Push_WH-00

LED Indication

Pairing

User Action

LED Indication

Status

Press the push button 3 times

LED blinks amber per second.

Pairing mode is active for 30 seconds. When pairing is completed, LED glows green for some time before turning off.

Resetting

User Action

LED Indication

Status

Press the push button 3 times and hold it down once for > 10 s.

After 10 s, the LED blinks red.

The device is in reset mode. It is reset to the factory settings after 10 seconds. The device then restarts and the LED blinks green for a few seconds and then stays amber.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.