DUG_SmartDim MW Push_WH-01

Resetting the device

You can reset the device to factory default manually.
  • Short press push button 3 times (< 0.5 s) and then long press the push button once (>10 s).

  • After 10 s, the LED starts blinking red and then release the push button.

  • The LED stops blinking upon successful reset of the device.

  • The Push-button Dimmer restarts and blinks green for a few seconds.

NOTE: After reset, the LED turns amber indicating that it is ready for pairing.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?