DUG_SmartDim MW Push_WH-01

Adjusting the brightness level using app

  1. On the Control tab, tap All devices or the room tab where the dimmer is located.
  2. On the Device Control Screen, drag the slider bar up/down to increase/decrease the brightness (A).
    TIP: Tap (B) on the Device Control Screen to turn the dimmer on/off.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?