DUG_SmartSwitch Push Wireless_WH-00

Resetting the device

You can reset the Wireless switch to factory default manually.

To reset the Wireless switch:

  1. Remove the rocker.
  2. Short press the top-right push button 3 times (< 0.5 s) and then press and hold the push button (>10 s).
    After 10 s, the status LED blinks red.
  3. Release the push button.
    • The status LED stops blinking upon successful reset of the device. 

    • The Wireless switch restarts and blinks green for few seconds. After reset, the status LED turns off.

    NOTE: All configuration data, user data, and network data are deleted.
  4. Assemble the rocker on the Wireless switch.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?