ESXP2GE016EN-05

Application Outcomes

Live Data Display

At any time, circuit breaker protection settings can be viewed in device diagrams.

Events and Alarms

Alarms are generated when circuit breaker trip settings change.

Reports

For each protective device, the Circuit Breaker Settings report displays the name, type of protection, and related thresholds.

It also detects any changes made with respect to a baseline.

Notifications

SMS and/or email notifications can be sent upon settings changes to help detect potential loss of selectivity.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?