ESXP2GE016EN-05

Data Recording and Timestamping

Circuit breaker protection settings data is recorded and timestamped by the Edge Control software (EcoStruxure Power Monitoring Expert or Power Operation). Therefore, no specific device for time synchronization is necessary.

For a comprehensive overview of device recording and timestamping capabilities, refer to Data Recording and Time Synchronization Capabilities of EcoStruxure Power Connected Products.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?