ESXP2GE016EN-05

Data Processing

Baseline Comparison*

A circuit breaker protection setting baseline is used by the Edge Control software (EcoStruxure Power Monitoring Expert or Power Operation Module) to compare the actual state of the circuit breaker settings to a baseline point in time.

If a change is detected between the state of the settings today and the state of the settings on the baseline date, the change will be timestamped, an event will be generated, and the change will be noted in the reporting.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?