Outputs
Outputs are displayed by the Edge Control software (EcoStruxure Power Monitoring Expert or EcoStruxure Power Operation).
Live Data Display
The protection settings (default trip curve) for a supported circuit breaker can be displayed in the default device diagrams of the Edge Control software.
Events and Alarms*
Any potential changes to the designed protection settings for a circuit breaker can be raised as an event or alarm in the Edge Control software’s native alarm interface.
By default, alarms are generated in case of any changes to the following settings:
-
Type of Protection
-
Long Time Overcurrent Protection Enabled
-
Long Time Overcurrent Pickup Threshold / Time Delay
-
Long Time Overcurrent Curve
-
Short Time Overcurrent Protection Enabled
-
Short Time Overcurrent Pickup Threshold / Time Delay
-
Short Time Overcurrent Curve
-
Instantaneous Overcurrent Protection Enabled
-
Instantaneous Overcurrent Pickup Threshold
-
Ground Fault Overcurrent Protection Enabled
-
Ground Fault Overcurrent Pickup Threshold / Time Delay
-
Ground Fault Overcurrent Curve
-
Earth Leakage Protection Enabled
-
Earth Leakage Protection Pickup Threshold / Time Delay
Reports*
Reports can be configured to be generated upon detection of a circuit breaker settings change.
Circuit Breaker Settings Report
Monitors and reports on the configuration settings of the circuit breakers in your electrical system. The report highlights changes between the baseline and the last known values.
The contents of the report can be summarized as follows:
-
Circuit breaker name
-
Protection settings, protection modes, maintenance status
-
Value (actual and baseline)
-
Date/time of change detection
-
Date/time of last settings verification
Notifications
Notifications of events and alarms can be sent by EcoStruxure Power Monitoring Expert or Power Operation using the Event Notification Module.