ESXP2GE0074EN-05

Digital Architecture

The digital architecture of the Guided Procedures Through Extended Reality application involves collecting the input data from the different products (including third-party), either directly over Ethernet, via gateways (such as EcoStruxure Panel Server), or through the EcoStruxure CPMA (Critical Power Management Appliance). This data is then passed to the EcoStruxure XR Operator Advisor Server for data processing. Data can then be viewed on different EcoStruxure XR Operator Advisor Client Apps.

The recommended digital architecture for the application is shown below:

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?