ESXP2GE0074EN-05

Application Outcomes

Contextual Asset and Site Information

Points of interest can be configured and virtually displayed in front of equipment and devices to communicate site-specific safety and maintenance information and to access drawings, user guides, and multimedia.

Overlaid Live Data

Device and equipment data can be virtually overlaid on equipment and viewed in the EcoStruxure XR Operator Advisor Client Mobile App and/or Desktop App, or through mixed reality glasses.

Overlaid Events and Alarms

Abnormal conditions are virtually overlaid on top of equipment and are highlighted to alert and guide users.

"X-Ray" Vision

Users can virtually look inside enclosures without the risks involved with opening doors or removing panels.

Step-by-Step Guidance

Users have access to generic or site-specific procedures with step-by-step instructions.

Data-driven step prerequisites can be configured to help ensure conditions are met before the next step can be started. Prerequisites can be status feedback from connected devices and/or pictures taken to document that actions were taken.

Remote Collaboration

A remote expert can support on-site personnel using the extended reality environment.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?