Data Recording and Timestamping
For the Guided Procedures Through Extended Reality application, a timestamp accuracy of ±1 second is sufficient to provide updated data to the user and monitor his actions.
Data recording and timestamping can occur at various levels for event data (status change, alarms, user actions, etc.) as well as for measurement data. Connected products, depending on the level of sophistication, can record and timestamp data as follows:
-
Event and measurement data recorded and timestamped on board: power meters such as PowerLogic ION9000, PM8000, HDPM6000, and some PowerLogic PM5000 models (PM53xx and PM55xx)
-
Event data recorded and timestamped on board, measurement data not recorded onboard: protection devices (PowerLogic P5/P3, MasterPacT MTZ, ComPacT NSX), ATS/PTS (ASCO 7000 Series PTS, TransferPacT Active Automatic), ATS controller (PowerLogic T300), UPS (Galaxy VX/VL/VM/VS), power correction devices (PowerLogic PFC and AccuSine PCS+/PCSn/EVC+/PFV+), VSD (Altivar)
-
No onboard recording at all: some energy/power meters (entry-level PowerLogic PM5000 models, Acti9 iEM3000, Acti9 Active, PowerLogic PowerTag), environmental sensors (PowerLogic TH110, CL110, HeatTag)
When EcoStruxure CPMA (Critical Power Management Appliance) is part of the architecture:
-
All data recorded and time-stamped onboard connected products are retrieved with their original timestamp and recorded by EcoStruxure CPMA.
-
Data which are not recorded onboard connected products are also retrieved but as real-time data. Recording and timestamping is carried out by EcoStruxure CPMA. The EcoStruxure XR Operator Advisor Server then connects to the EcoStruxure CPMA as a single data source to overlay status, alarms, and measurements in the EcoStruxure XR Operator Advisor Client Apps.
When EcoStruxure CPMA is not part of the architecture: EcoStruxure XR Operator Advisor Server must connect directly to all connected products to retrieve status, alarms, and measurements as real-time data and overlay them in the EcoStruxure XR Operator Advisor Client Apps.
During the execution of procedures, the EcoStruxure XR Operator Advisor Server records and timestamps all user steps with their duration.
For a comprehensive overview of device recording and timestamping capabilities, refer to Data Recording and Time Synchronization Capabilities of EcoStruxure Power Connected Products.