ESXP2GE0074EN-05

Data Processing

Data processing is performed by the EcoStruxure XR Operator Advisor Server. Data collected can be compared between communicating devices and/or to configured thresholds.

Trigger conditions calculated by the server use these data comparisons to determine if an operator can move to the next step of a procedure.

Additionally, the relative location of operators is calculated and can enable spatial trigger conditions that help prevent an operator from proceeding unless he or she is in the correct position.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?