0100DB2304

Implementation for Busway

For each busway joint or junction, such as tap-off points, corners, elbows, or joint packs, a single PowerLogic CL110 is installed*. Per-phase sensors are not required. Continuous Thermal Monitoring for busway only uses the EcoStruxure Panel Server to wirelessly collect data from PowerLogic CL110 Environment Tag. A Substation Monitoring Device (SMD) is not required.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?