0100DB2304

Implementation for LV Switchgear

In LV Drawout Switchgear, up to 65 sensors can be installed to monitor each phase at the following customer connection locations:

  • Customer Incoming Phase Connectors of Mains 1

  • Customer Outgoing Phase Connectors of the Feeders 2

As an option, one PowerLogic CL110 per section can be added for ambient temperature measurement.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?