0100DB2304

Wireless Data Concentration

In the Continuous Thermal Monitoring application, the wireless signals from the temperature sensors are collected by a wireless data concentrator:

  • For MV switchgear and MV/LV transformers, depending on the offer, the Harmony ZBRN32 or the EcoStruxure Panel Server is used as the data concentrator. Up to 60 sensors can be connected per ZBRN32 or 85 per Panel Server.

  • For LV busway, the EcoStruxure Panel Server is used as the data concentrator. Up to 65 sensors can be connected per Panel Server.

  • For LV switchgear, the EcoStruxure Panel Server is used as the data concentrator. Up to 65 sensors can be connected per Panel Server.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?