990-91385F-001

Model List

  • G3LUPS250KHTS: Galaxy 3L 250 kVA 400 V, TLC-Certified, start-up 5x8

  • G3LUPS300KHTS: Galaxy 3L 300 kVA 400 V, TLC-Certified, start-up 5x8

  • G3LUPS400KHTS: Galaxy 3L 400 kVA 400 V, TLC-Certified, start-up 5x8

  • G3LUPS500KHTS: Galaxy 3L 500 kVA 400 V, TLC-Certified, start-up 5x8

  • G3LUPS600KHTS: Galaxy 3L 600 kVA 400 V, TLC-Certified, start-up 5x8

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?