990-91437A-001

Configure the Input Contacts and Output Relays

  1. From the home screen of the display select Settings > Advanced settings > Contacts and relays .
  2. Select Enable or Disable for the following features:
    • Backfeed on input

    • Battery breaker trip

    • Backfeed on bypass

    • External MBB status

  3. Tap arrow down and set the function for each of the configurable output relays. Note that there are two screens for output relays. Choose between:
    • Disable

    • Common alarm

    • In normal operation

    • On battery

    • Static bypass

    • Maintenance bypass

    • Output overload

    • Charging


    • Fan inoperable

    • Battery inoperable

    • Battery disconnected

    • Battery voltage low

    • Input out of tol.

    • Bypass out of tol.

    • EPO active

  4. Tap arrow down and set the function for each of the configurable input contacts. Note that there are two screens for input contacts. Choose between:
    • Disable

    • INV ON

    • INV OFF

    • Battery inoperable

    • Genset on

    • Custom alarm 3

    • Custom alarm 4

    • Disable ECO

    • Force INV OFF

    • Force charger OFF

  5. Tap Save settings.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?