990-91437A-001

Transfer a Parallel System from Normal Mode to Maintenance Bypass Mode

  1. From the home screen on the display select Control > Inverter ON/OFF > Turn par. INV OFF .

    All UPSs will turn to static bypass mode.

  2. Turn the maintenance bypass breaker MBB to the ON (closed) position.

    The load is now supplied via the maintenance bypass breaker MBB.

  3. Turn the battery breakers BB of all UPSs to the OFF (open) position.
  4. Turn the unit input breakers UIB and the static switch input breakers SSIB of all UPSs to the OFF (open) position.
  5. Turn the unit output breakers UOB of all UPSs and the system isolation breaker SIB to OFF (open) position.
DANGER
hazard of electric shock, explosion, or arc flash
  • Wait at least 5 minutes before removing the cover of the UPS after the display has turned off to allow for the capacitors to fully discharge.
  • Always measure for hazardous voltages on all terminals before working on the UPS.
Failure to follow these instructions will result in death or serious injury.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?