990-91437A-001

Remote EPO

Only use the remote EPO in case of emergency.

When the remote EPO is activated, the UPS will:

  • By default: Turn off the rectifier, inverter, charger, and static bypass and stop supplying the load immediately, or

  • Configurable: Transfer to static bypass mode and keep supplying the load.

DANGER
hazard of electric shock, explosion, or arc flash
The UPS control circuit will remain active after the remote EPO has been activated if input is available.
Failure to follow these instructions will result in death or serious injury.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?