Safety Precautions
![]() |
---|
Hazard of electric shock, explosion, or arc flash
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
Storage
NOTICE |
---|
RISK OF EQUIPMENT DAMAGE
Batteries should not be stored beyond 15 months from the
date of production. If they are stored for longer the calendar degradation
will cause the batteries to be irreversible degraded beyond what is
expected – a reduced runtime will be the consequence.
Failure to follow these instructions can result in equipment damage.
|
If the equipment is to be stored prior to installation, it should be stored in a cool, dry, well-ventilated location that is protected against rain, splashing water, chemical agents, etc. The equipment should be covered with a tarpaulin or plastic wrapper to protect it against dust, dirt, paint, or other foreign materials.