990-915454A-001

Communication and Management

Local area network 100 Mps
Communication protocols Modbus TCP/IP, Ethernet, RS485, SNMP
Control panel 7-inch touchscreen display
Audible alarm Yes
Emergency power off (EPO) Yes
Connectivity StruxureWare for data center operation
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?