990-66228A-001

Configure the Backfeed Protection Settings for the Unit Input Breaker UIB on the UPS Display

  1. From the main menu of the UPS display, select Settings > Advanced settings > Dry contact settings > Output dry contact.
    NOTE: The Settings menu requires administrator login to access. The default password is ‘000000’.
  2. Select the output dry contact for configuration that you connected the backfeed shunt trip cables to during installation.
  3. Set the Status of the output dry contact to Closed and the Function to Backfeed on input.
  4. Tap Confirm to save your settings.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?