990-66228A-001

Specifications

Torque Specifications

Bolt size Torque
M2 0.3 Nm
M3 1 Nm
M4 2.5 Nm
M8 12 Nm
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?