990-66228A-001

Configure the Backfeed Protection Settings for the Static Switch Input Breaker SSIB on the UPS Display

  1. Start up the UPS - follow the instructions in the UPS operation manual.
  2. From the main menu of the UPS display, select Settings > Advanced settings > Dry contact settings > Output dry contact.
    NOTE: The Settings menu requires administrator login to access. The default password is ‘000000’.
  3. Select the output dry contact for configuration that you connected the backfeed shunt trip cables to during installation.
  4. Set the Status of the output dry contact to Closed and the Function to Backfeed on bypass.
  5. Tap Confirm to save your settings.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?