990-6317G-001

Communication and Management

Local area network 100 Mps
Communication protocols Modbus, TCP/IP, Ethernet, RS485, SNMP, BACnet/IP
Control panel 7-inch touchscreen display
Audible alarm Yes
Connectivity StruxureWare for data center operation
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?