990-6317G-001

Compliance

Safety UL 60950-1 and CAN/CSA C22.2 No. 60950-1-07 Information Technology Equipment – Safety – Part 1: General Requirements
UL 891, Switchboards, Edition 2
CSA C22.2 No.244:19, Switchboards, Edition 2
EMI/EMC/RFI FCC Part 15, Subpart B, Class A
Marking cULus
Seismic ICC ES AC156, HCAI (formerly OSHPD) Pre-Approved, Sds=1.64 g for z/h=1, z/h=0; Ip=1.5
Protective class I
Pollution degree 2
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?