990-91397B-001

Shipping Weights and Dimensions

Commercial reference Weight kg (lbs) Height mm (in) Width mm (in) Depth mm (in)
GRPPNQ84 230-280 (507-617) 2261 (89) 1066 (42) 1066 (42)
GRPPIP2X84 2261 (89)
GRPPNF84 2261 (89)
GRPPNQ89 2388 (94)
GRPPIP2X89 2388 (94)
GRPPNF89 2388 (94)
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?